WITTENSTEIN SE at sps ipc drives 2018
WITTENSTEIN SE’s clear focus on technical solutions – in all their complexity – will be at the center of the Group’s exhibit at the upcoming “sps ipc drives” from November 27 to 29, 2018 in Nuremberg. Among other things, WITTENSTEIN’s various Business Units create user and application-specific solutions by consistently modularizing components and systems, through end-to-end project support combined with a high level of vertical integration and by implementing innovative and sustainable concepts in the fields of mechatronics and connectivity.
WITTENSTEIN alpha GmbH, for example, will be unveiling the new CP gearboxes in the alpha Basic Line along with the new, space optimized right-angle stages for both this series and the alpha Value Line. The stylish bevel gear stage, designed for use in tight mounting situations, impresses with compactness and high efficiency. Owing to the market-compatible output interfaces, the extensive range of possible coaxial and right-angle versions is suitable for a wide variety of tasks.
The further expanded, industrial grade toolkit for small servo drives – the cyber® dynamic line in combination with the cyber® simco line with the fieldbus interfaces PROFINET RT/IRT, EtherCAT, Sercos III, EtherNet/IP and CANopen – means that more than 12,000 different customer and application-specific motor-controller combinations can now be configured. If this is not sufficient, WITTENSTEIN cyber motor GmbH can seize the opportunities afforded by high vertical integration to develop customized solutions with customer-specific motors and thus deliver the right customer value without any design limitations – whether for standard applications or for extreme environments.
In keeping with the motto “Focused on your needs”, WITTENSTEIN will be offering a guided tour at the booth on the subject of Smart Connectivity: more and more companies are meanwhile recognizing the need for intelligent connectivity solutions, which are a vital prerequisite to cutting-edge automation.
Passend zum Motto „Focused on your needs“ bietet WITTENSTEIN auf dem Stand eine Guided Tour zum Thema Smart Connectivity an, denn immer mehr Unternehmen erkennen den Bedarf an intelligenten Konnektivitätslösungen, ohne die eine zukunftsweisende Automation nicht denkbar ist.
Photo
Right-angle gearbox in the new CP series from WITTENSTEIN alpha.