WITTENSTEIN at SPS 2023: Innovations in the cybertronic product world
The goal: to play a key role in shaping digital transformation in drive technology and machine construction. With this in mind, WITTENSTEIN is now transferring the functionality of selected mechatronic products and systems – with integrated electronics, sensors and firmware – to cybertronic products and systems that can also communicate and interconnect with each other. WITTENSTEIN’s Smart Services, such as the smart Anomaly-Check function, further expand the solution space of these products and systems, providing an easy way to analyze and process machine data.
Digitalization is so easy
Gearboxes with cynapse® functionality collect operating data independently from machines and plants and communicate it in the IIoT.
Smart Services add functionality to the cynapse® feature. The three basic functions are data collection, visualization and analysis. The core know-how that WITTENSTEIN has built up over 40 years of developing low-backlash planetary gearboxes, in combination with operating data, enables a gearbox’s condition to be computed and displayed in the Smart Services.
In the end, it’s the added value for customers that results from cynapse® and the Smart Services that is the decisive factor. Condition monitoring and predictive maintenance help to avoid failures or detect anomalies before it’s too late.
Galaxie® gearbox: Portfolio expanded and restructured with “accuracy line” and “robustness line”
The upcoming exhibition will simultaneously mark the “product premiere” of the Galaxie® gearboxes in the “accuracy line” series. The kinematics, bearing, ratios and even larger hollow shaft diameters were specifically designed to meet the requirements of high-precision applications. The series additionally includes miniaturized gearbox variants that are installation-compatible with strain wave gearboxes in terms of dimensions. The new series is available in five different sizes and rated for maximum torques of 150 Nm to 6000 Nm.
To coincide with the market launch of the Galaxie® accuracy line, the proven variants of the Galaxie® gearbox have been united in the Galaxie® “robustness line” series. They share the same nominal torque, outer diameter and torsional rigidity values, but with their better overload capacity and more robust bearings they are targeted at applications with higher mechanical requirements.
Both product lines come in several product variants – flange, hollow shaft and right-angle gearboxes as well as compact servo actuators. All Galaxie® gearboxes have identical DNA: with their zero backlash, maximum torsional rigidity, high torque density, extremely smooth running and large hollow shaft, they set the standard in the market for precision gearboxes.
Frameless servo motor family expanded with cyber® kit line medium
The cyber® kit line product family has just gained a new member: this frameless motor series has been expanded with the new cyber® kit line medium in sizes 100 and 112. These torque-optimized, highly integrated motors score with their compact design and high torque density. Versions with either a small or a large hollow shaft are available. The modular toolkit provides enormous design flexibility with different sizes, lengths and voltage classes for 60 V and 600 V applications. The motor series is moreover compatible with the cyber® simco® drive 2 servo drive.
As highly dynamic drive solutions, these rugged frameless motors have proven themselves in robotics, machine tools, actuators, testing and measurement technology and semiconductor manufacturing, amongst others.
The new cyber® kit line medium is the perfect complement to the successful cyber® kit line small and large series.
Picture (source: WITTENSTEIN SE):
Galaxie® accuracy line: New Galaxie® gearbox series with 4 product variants